How can we replace the case assembly of the modular F.R.L units?
What is the part No. of the filter element of the AF unit for the AC modular units?
Can we mount a round face pressure gauge later on the regulator for the AC∗∗ modular units?
How can we order the cross spacer, piping adapter and pressure switch with piping adapter as an attachment for the AC modular units?
Is there any limitation of the mounting orientation of the AC modular units?
During the model selection of the AC modular units, how should we determine if the lubricator is necessary or not?
Could you tell me when the AR regulator series was redesigned and released?
Do you have a non-grease type or oil-free type for the AR regulator?
Why is a set nut not supplied together with AR regulator of the part number AR∗∗-∗∗-A?
Could you tell me when the AF filter series was redesigned and released ?
Can I attach elements of the old AF and AFM products to the new products?
Is there interchangeability if we want to replace a part of the 2-digit conventional modular units with a refresh unit during maintenance work?
We would like to replace a regulator of AC 10-60 unit during the maintenance. We want to mount the new AR∗-B (-B at the end of the model. No) Are they interchangeable?
How can the AF40-03-A and AFM40-03-A modularly connect with an IR3000-03-A (or IR3200-03-A)?
In the WEB catalogues on the SMC homepage there are some product with "10-" and "25A-" before the series. What does this mean?