Can I press fit an inch size tubing with a specialized tool of the LQ1 series?
Is a specialized jig required when piping a LQ1 or LQ3 product?
I bought an insertion tool for the high-purity fluoropolymer fitting. Could I have any information for press fitting methods?
Which pilot ports should I use for the valve types, N.C., N.O. and Double acting, in the LVA, LVC and LVD series?
Is there any restriction on the mounting orientation of the LVA, LVC and LVD products? I would like to mount these products horizontally on the wall.
A resin material is used for the female threaded part of the resin body types PPS and PFA in the LVA products. Can I use a metal thread fitting for mating with the resin thread types?
What is the suck back valve in the LVC23 series?