Are there any instructions of setting ZSE/ISE30A, 40A and 80 avilable ?
What is the display resolution in ISE30A? What is the display resolution in ZSE30A(F)?
How should ISE30A be used only to indicate numerical values?
Is calibration for the pressure switch available?
What is the sampling cycle for the digital display?
How can I stop displaying Hi and figure alternately?
Is a pressure switch with an IP65 enclosure available?
Can the 2-colour display of ISE30A/40A/80 series be set from the status of OUT2?
Is there any rule for the hysteresis setting?
What is the auto shift function for ZSE80?
When using the ZSE80 only for confirmation of pressure, is there any way to prevent the OUT1 and OUT2 indicators on the display flashing?
What is 1 digit?
Is pressure switch with the absolute standard available?
How can Zero Clear Function be used for display in ISE/ZSE?
How can ISE10/30A/40A/80 series be set back to the default (factory default) ?
Vacuum pressure switch, ZSE series can reach out of the applicable pressure due to vacuum break (purge). Isn't it broken?