Are there any instructions of setting PF2A, PF2W and PF2D avilable ?
Regarding PF2A series, is the displayed value (L/min) standard or normal one?
If the PF2A721 is in window comparator mode, and the hysteresis is 3 digits what flow rate is this equivalent to? Also what is the resolution of the displayed flow rate when in instantaneous flow mode?
When PF2A712H-20-28M indicates "---", which action should be taken?
How should we carry out wiring when using PF2A7 series just to check the flow rate display?
What is the diameter of straight piping of IN side?
Do you have detailed data concerning the flow rate and temperature setting for the PF3W series?
I am currently selecting an integrated display type of the PF3W series. Can the PF3W7 series only provide an analog output for either flow rate or temperature?
What is the relationship between the analog output and the flow range of the PF□ series?
“Troubleshooting” is set out in the operation manual that comes with a PF□ series product, but do you have detailed data concerning troubleshooting?
I wish to select a flow sensor. Is there an easy selection method?
Can I use a fluid (gas) other than dry air in a PF□ series product?
Can I use a fluid (liquid) other than water in a PF□ series product?
Are there PF□ series products with lead wires that are longer than the standard ones?
Please tell me how to wire PF□ series products.
Roughly what length of straight pipe should be used on the IN side of a PF□ product?
Is it possible to install a PF□ series product vertically?
Is the flow rate display of the PF□ series product for air converted into atmospheric pressure (standard condition)?
What kind of output is the accumulated output mode and the accumulated pulse output mode of the PF□ series?
In the PF3W711 type, the P_1 setting (normal output and hysteresis mode) cannot be reduced to 12 L/min or less. Why?
What is the order of accuracy of the PFMB7 series?
Can I use a PF□ series product on the flow rate display alone, without using the switch function?
The letters [HHH] are indicated on the PF□ series product. (In the case of PF2□, [---] is indicated.)