What should be selected as an angle adjustment unit if we want to mount it on the CRB2, CRBU2, and CRB1series later?
What is the backlash of the rotary actuator (rack and pinion type)?
We cannot rotate the CDRB2BWU series by hand or even if we are applying pressure. What is the problem?
If we want to adjust the angle to 180゜with the CRB2BWU sizes 10 to 40, do we need to select the 270゜rotating angle type?
Can we replace the packing of CRB, rotary actuator vane type as internal leakage is increasing.
Where can we find the effective torque and air consumption of the CR∗/MS∗ series?
Do you have model selection software for the rotary actuators?
Can we stop the rotation by using the (closed center) valve?
Can we change from the MSQ∗ sizes 10 to 200 A (adjustment bolt type) to the MSQ∗ sizes 10 to 200 R (internal shock absorber type)?
The MSQ∗30A rattles when we adjust the angle to 90゜and apply external force at rotation end against rotation movement. Is it backlash of the gears?
Do you have a product that can rotate 90゜to both the right and left sides?