Should I use a 2 or 3 wire type solid state auto switch?
What is the current model type of the old type D-F9B autoswitch?
We would like to purchase an auto-switch only for the CDQ2B32-30DMZ-M9BW cylinder. Which auto-switch models can be ordered as stand-alone products?
There is a product number on the D-M9B auto-switch part and after this there is 3 alphabetical letters. What do these 3 letters mean?
Please give the part number suffixes for auto switch lead wire lengths of 0.5m・3m・5m.
Please tell me the auto switch labelling methods for the pre-wired connector accessory and pin layouts.
What is the flex resistance of the cable for autoswitch D-M9∗ series?
What are the detailed specifications of the cable (lead wire) for D-M9□ series solid state autoswitch?
Please tell me the auto switch operating range.
What is the difference between the standard product and the improved water resistance auto switch?
What is the difference between reed and solid state auto-switches?
Please tell me the auto switch wiring method.
I would like to mount an auto switch to a cylinder with a built-in magnet. Where in the catalogue are the auto switch mounting bracket part numbers listed?
Where is the cylinder auto-switch in the WEB catalogue? This is to confirm the auto-switch specifications.
Are there 2 kinds of auto switches D-M9□, round lead wire and oval lead wire ?