What is the bleed of precision regulator IR?
I have a question regarding the precision regulator IR series. The supply pressure is 0.5 MPa and the set pressure is 0.2 MPa, however, air is leaking from a small hole in the main body.
What does the sensitivity "within 0.2% of full span" in the catalog specification in Precision Regulator IR series mean ?
Is it possible to mount an IR1000/2000/3000 product in a panel mount?
Is it possible to install an IR series product between the cylinder and the solenoid valve?
What is the difference between the IR, IR-A and ARP precision regulators?In addition, what is the difference between the IR-A regulators (IR1200-A/IR2200-A/IR3200-A)?
How can the AF40-03-A and AFM40-03-A modularly connect with an IR3000-03-A (or IR3200-03-A)?
Are there any product with the set screw piping in IRV series?
How can it possible to mount a KQ2 product to the point where the gauge of IRV should be mounted? It is hexagon shape without ridges.
Does ITV has a gauge port?
There is a buzzing noise from the ITV when the power is ON with no air supply or no input signal. What is the problem?
What does "Er.1 (Error 1)" of ITV2030-222BS mean and how can we solve it?
Is there a power cable, other than the standard 3-meter long cable, available with ITV1000 to 3000 series?
Is a cable connector enclosed with the CC-Link and DeviceNet ITV?
Can we install an ITV unit between a cylinder and solenoid valve?
There is a caution statement that "OUT pressure will be retained temporarily when the product is in a controlled state even if the power is cut off". What does it mean?
What is the M5 threaded hole at the front of the ITV20∗∗/30∗∗ for?
Which (ITV2000 or 3000) does SMC recommend if we want to deliver pre-set pressure only?
What is the minimum outlet pressure resolution of ITV2010?