What is the operating pressure differential of a 2 port valve?
What is the difference between the valve types N.C. and N.O. in the catalog for VX2 ? Also, how does the body material 'Al' differ from 'C37'?
Does the body have any indication for showing direction of flow in VX?
When VX2∗4 is used in vacuum, which port should the vacuum pump be connected with?
Is it possible to adopt C37 or SUS body when New VX2 is used for air?
Is there any applicable 2 port valve with the port size Rc3/4 in VX series to perform air blow?
What is the polarity to wire the VX product (2 port solenoid) at DC24V?
We are considering using VX product energizing for a long time. Would it be no problem, if we will pay attention to heat of the body?
Is it possible to use VX3 product with 3 port valve as a divider valve? Fluid: water
Where in the SMC website is catalog for discontinued 2 port valves located?
I want to select a 2 port valve. Is there any data available for selecting an appropriate valve?
What is the meaning of the numbers and letters of the alphabet in How to Order of the new VX2, VXD and VXZ series?
What is the power consumption of the new VX2, VXD and VXZ series?
When I inquired about the existing VX2330 for use with air that is currently being used, I was told that it was the same as the VX222A. The catalog states that this product is for use with water. Is it possible to use the VX222A series, which has a brass body, for use with air? Also, is there any difference in the amount of air leakage from a valve with an aluminum body compared to one with a brass body?
I purchased a VX230GA and installed it in order to use it for an air blow, but air did not come out from the secondary side. The factory air pressure is 0.4 MPa, and voltage is applied, but the valve does not open. When I disconnected the primary side air piping, the valve opened. Is the supply pressure too high? Does this trouble occur because the maximum operating pressure difference of the VX230GA is 0.1 MPa?
What are the part numbers of the new VX2, VXD and VXZ series with bracket?
Can I install a bracket on the new VX2, VXD or VXZ series after purchasing it?
Please tell me how to wire the new VX2, VXD and VXZ series.
What will happen if the pressure on the OUT side of a VX series 2 port N.C. type valve becomes higher than the pressure on the IN side?
Is there any restriction on the mounting orientation of the VX□ series?
I would like to change the electrical entry direction of the new VX2, VXD and VXZ series.