Why does a 5 port solenoid valve not work correctly with low pressure (0.1 MPa)?
What are the differences between metal and rubber seals fitted to valves?
In the WEB catalogues on the SMC homepage there are some product with "10-" and "25A-" before the series. What does this mean?
Is the SYJ series interchangeable with the VJ series?
What is the difference between the conventional SY series and the new SY series?
What is the part number for the SY series connector assembly with L / M type plug connector?
What is the assembly number of the blanking plate for SY manifold (SS5Y∗)?
When connecting SY solenoid valves to DC voltage, are the connections polarity sensitive?
What is the O.D of the outer sheath and the cross section of the conductor for the lead wire of the solenoid valve?
Regarding SY series DIN terminals, what is the difference between D and Y?
Using the HP ""CAD Data Search"" feature, how can the 2D-CAD data for the SY5140-5LZ-02 be found?
We use SY5120-1G-C6 but we began to notice air leakage from the EA port. It has been used for 5 years as a cylinder drive.
In the code VF3130-1G1-02, what is the meaning of the 1 after the '1G'?
What changes have been made to VF1000, 3000 and 5000 series after the model changeover?
How should I use the external pilot type (Pilot type R) in VP300/500/700 series?
Is there polarity for connecting electrical wiring to the DC type of the VP300/500/700 series?
How can I change N.C. valve type to N.O. type in the VP300/500/700 series?
What is the part number of the connector assembly for the part number VP542-5MOZ1-03A?
What is the meaning of: "a single valve with 6 valve functions (universal porting type)" of the VT3∗∗ series?
How should I configure piping of the VT307V series in the vacuum line in order to hold the work piece when energised and release the vacuum when de-energised?
Where can I find VO307 on the SMC website.
What is polarity of the VT3∗∗ series (DC type)?