In what section of the operation manual of the HRS series are there details of serial communication (RS232C, RS485)?
It is stated that the circulating fluid used in the HRS series is tap water or 15% ethylene glycol aqueous solution. Can I use town water or deionized water?
Is the D-sub connector for communication with the main body of the HRS series male or female? Also, what is the size of the screws used to fix the D-sub connector?
With the HRS series, the circulating fluid is set to a temperature of 30℃. However, the temperature of the circulating fluid does not stabilize. The set environment and power source are within the range of the specifications.
Is it possible to adjust the circulating fluid discharge flow when using the HRS series?
What is the recommended capacity of the earth leakage breaker to be installed when using a HRS series product?
Does SMC handle 15% ethylene glycol aqueous solution?
Can I directly flow fluid whose temperature I wish to control (e.g. cutting oil, seawater, etc.) from the return port of the chiller to the discharge port?
Is it possible to control the temperature with the HRS series, using tap water in an open type external tank as the circulating fluid?
The alarm lamp on the HRS□□ flashed, and the alarm No. AL□□ appeared. What is the nature of this alarm?
How do you turn the HRS□□ ON/OFF by remote operation?