Is it possible to use KQ2 series with water as fluid?
What is the difference between the existing KQ2 series and refreshed KQ2 series?
What is the difference between KQ2H06-01AS and KQ2H06-01NS?
KJ series has been integrated into the new KQ2 series. What are the existing model no. of KJL04-M3 and KJL06-01S?
Is there a black body available in new KQ2 series?
We want to use φ8 and φ12 tubes inside and outside of the panel. Are there bulkhead fittings with different diameters available?
Figures 8 and 5/16 are imprinted on the release bushing of KQ2 as well as SMC marking. What do these two figures mean?
Is it possible to connect metal tubing (SUS, copper tubing, etc.) to one-touch fittings?
What is the tightening torque of the connection thread for KQ2 series one-touch fittings?
Are there fittings for mm size tubing and with NPT connection thread?
Are there fittings resistant to 100℃ heat?
Is it possible to rotate the body of KQ2L and KQ2Twhere tubing is inserted after tightening the connection thread?