Support / Contact Us »
FAQ

|Air Cylinders

What is the A stroke/B stroke of the dual stroke cylinder/single rod type (-XC11)?

The stroke order in the model name is shown as A (rear cylinder) + B (front cylinder). The total stroke is the sum of the strokes indicated.
Calculation of total stroke (B cylinder)
E.g.) CM2B32-25+25-XC11 ⇒ 25+25=50
Basic Condition ①・・The stroke of the front cylinder must be longer than A (rear cylinder)
Reason・・After the A stroke, if there is no remaining stroke, the multiple stages cannot be completed.
Basic Condition ②・・The range in which double output can be achieved is within the A (rear cylinder) stroke.
Reason・・If there is no reactionary force (work piece), within the A stroke range, this cannot be achieved.