Documents / Download » Model Selection Software »
Power Clamp Cylinder Model Selection Software »
Power Clamp Cylinders Model Selection Software Install
Power Clamp Cylinders Model Selection Software
∗ The software (Download ver. or Web ver.) is available free of charge.
Please check the software precautions before use.
How to Install Selection Software
The following describes the installation procedures by taking the Shock
Power Clamp Cylinder selection software as an example.

- 1. Save the compressed file you have
downloaded into a folder.

- 2. Extract the compressed file.
- Extract the compressed file in the ZIP
format. When you extract “Power Clamp Selector.zip”,
the “Power ClampSelection ****” folder is then
created.

- 3. Start the installation
-
Open the “Power ClampSelecor ****” folder.
Double-click “SETUP.EXE” in the folder
to start the installation.

- 4. Installation screen
- Select a language and click [OK].

- The Setup Wizard will start up. Click [Next].

- Check the installation destination and click [Next].

- Click [Install] on the Installation screen.

- The installation will start running.
- 5. Complete the installation
-
When the installation has been completed, the icon to run this
software is created on the desktop. Additionally, as [Start] →
[Programs] → [SMC Application] → [Power Clamp Selector] is
registered, you can also run this software from these selections.
The installation is then completed.