Documents / Download » Model Selection Software »
Charge and Discharge to/from Tank Calculation Software »
Charge and Discharge to/from Tank Calculation Software Install
Charge and Discharge to/from Tank Calculation Software
∗ The software (Download ver. or Web ver.) is available free of charge.
Please check the software precautions before use.
How to Install Selection Software
The following describes the installation procedures by taking the Charge and
Discharge to/from Tank Calculation Software as an example.
- 1. Save the compressed file you have
downloaded into a folder.
- 2. Extract the compressed file.
- Extract the compressed file in the ZIP
format.
When you extract “Charge to Tank
Calc.zip”, the “Charge to Tank Calc ****”
folder is then created.
- 3. Start the installation.
-
Open the “Charge to Tank Calc ****”
folder. Double-click “SETUP.EXE” in
the folder to start the installation.
- 4. Installation screen
- Select a language and click [OK].
- The Setup Wizard will start up. Click [Next].
- Check the installation destination and click
[Next].
- The installation will start running.
- Check that the installation has been
completed, and then click [Finish].
- 5. Complete the installation
-
When the installation has been completed, the icon to run this
software is created on the desktop. Additionally, as [Start] →
[Programs] → [SMC Application] → [Charge to Tank Calc] is
registered, you can also run this software from these selections.
The installation is then completed.