|
SMC Model
Selection Software Ver. 3.5 Web Version |
|
Ver.3.5.06
update July 8, 2010 This
is the entry page of the web version of the Model Selection Software Ver.
3.5. |
|
Run Model Selection Software Ver. 3.5 Click the alternative link below if you use a computer on corporate
networks. Run Model Selection
Software Ver. 3.5 (on SSL TYPE1) |
|
How to operate: |
|
Click
the above link "Run Model Selection Software Ver. 3.5", and
"ICA Web Client" will be automatically installed only for the first
time. After that a screen of the Model Selection Software will be shown in a
separate window. Click the "Exit" button in the screen of the
program in order to terminate the program. |
|
Notes: |
|
This
page is compliant with Internet Explorer 4.0 or later. Internet Explorer will
automatically install required "ICA Web Client" to connect our
server. This process will be done only once. |
|
In case of failure: |
|
If
the Model Selection Software will not be shown even if you use Internet
Explorer, install "Win 32-bit ICA Client" first and click the link
again. Just click "Next" or "Yes" for all steps in the
installation. |
|
Click here to
download Win 32-bit ICA Client |
|
|
|
Ver. 3.5
CD-ROM Version: |
|
CD ROM version download Please
download and use the latest version of the CD ROM program with the link
below. SMC Model Selection Software Ver.
3.5.06 download |
|
The data
update of the software The software before March 5, 2010
cannot update data by the system change. |