|
SMC Model
Selection Software Ver. 3.5 Web Version |
|
Ver.3.5.02 update
May 13 2009 This
is the entry page of the web version of the Model Selection Software Ver.
3.5. |
|
|
|
Run Model Selection
Software Ver. 3.5 Click the alternative link below if you use a
computer on corporate networks. Run Model Selection
Software Ver. 3.5 (on SSL TYPE1) |
|
|
|
How to operate: |
|
Click
the above link "Run Model Selection Software Ver. 3.5", and
"ICA Web Client" will be automatically installed only for the first
time. After that a screen of the Model Selection Software will be shown in a
separate window. Click the "Exit" button in the screen of the
program in order to terminate the program. |
|
|
|
Notes: |
|
This
page is compliant with Internet Explorer 4.0 or later. Internet Explorer will
automatically install required "ICA Web Client" to connect our
server. This process will be done only once. |
|
|
|
In case of failure: |
|
If
the Model Selection Software will not be shown even if you use Internet
Explorer, install "Win 32-bit ICA Client" first and click the link
again. Just click "Next" or "Yes" for all steps in the
installation. |
|
Click here to
download Win 32-bit ICA Client |
|
|
|
Ver. 3.5 download Version: |
|
The simple
download Version download The
simplified download program version will allow you to use the Model selection
program while accessing the Model Selection Program's database.
Download and decompress the file and then double click on the Mss.exe in the
file folder to begin the access process. In addition, it is possible to
print or save the resulting data with this program. |