SMC Pneumatic Energy Saving Program Ver.2 Web Version
This is the entry page of the web version of the Energy Saving Program Ver. 2.
Please note that the links may be sometimes missing due to maintenance of the server.
English version for United States of America
Run Energy Saving Program Ver.2 (Direct connection)
Run Energy Saving Program Ver.2 (Connection via a proxy)
Run Energy Saving Program Ver.2 (Connection via a HTTPS proxy)

English version for Europe union
Run Energy Saving Program Ver.2 (Direct connection)
Run Energy Saving Program Ver.2 (Connection via a proxy)
Run Energy Saving Program Ver.2 (Connection via a HTTPS proxy)
How to operate :
Click the above link "Run Energy Saving Program Ver.2", and "Citrix ICA Client" will be automatically installed only for the first time.
After that a screen of the Energy Saving Program will be shown in a separate window.
Click the "Quit" button in the screen of the program in order to terminate the program.
Notes :
This page is compliant with Internet Explorer 4.0 or later. Internet Explorer will automatically install required Citrix ICA Client to connect our server. This process will be done only once.
In case of failure :
1. When an Citrix ICA client is not installed automatically, please download from the following and perform manual installation.

Download Citrix ICA client@i3.68 Mbytesj

2. If our server is not connectable through corporate networks.

Please look at the check list here.

You cannot use our system if the required ports are blocked in your network for the security purpose.
In that case, please access through external ISP.