TOP2.GIF
TIT4.GIF
Mark of compliance for CSA/UL
CSA Standards & UL Standards

UL and CSA standards have been applied in North America (U.S.A. and Canada) symbolizing safety of electric products, and are defined to mainly prevent danger from electric shock or fire, resulting from trouble with electric products. Both UL and CSA standards are acknowledged in North America as the first class certifying body. They have a long experience and ability for issuing product safety certificate. Products approved by CSA or UL standards are accepted in most states and governments beyond question.
Since CSA is a test certifying body as the National Recognized Testing Laboratory (NRTL) within the jurisdiction of Occupational Safety and Health Administration (OSHA), SMC was tested for compliance with CSA Standards and UL Standards at the same time and was approved for compliance with the two Standards. The above CSA NRTL/C logo is described on a product label in order to indicate that the product is approved by CSA and UL Standards.

TSSA(MCCR) Registration Products

TSSA is the regulation in Ontario, Canada. The products that fall into the scope of the TSSA regulation are those with an operating pressure of more than 5 psi(0.03MPa) and a piping size larger than 1 inch diameter.


|HOME|MAIN MENU|SUB MAIN MENU|HELP|